AXIS#.MOTOR.BRAKECONTROL
Description
This command allows a user to release or apply the motor brake. If at any time, the command is unequal to 0, the warning W5001 is generated. The warning will be dismissed as soon as the command becomes 0 again.
| Value | Description |
|---|---|
| 0 | Axis controls the brake |
| 1 | Brake is released |
| 2 | Brake is applied |
-
- See the Brake help page for detailed information about brake control, including brake operation with a vertical load.
Examples
Code
-->AXIS1.MOTOR.BRAKECONTROL 0
-->BRAKE1.STATE
0
-->AXIS1.MOTORBRAKECONTROL 1
-->BRAKE1.STATE
1
-->AXIS1.MOTOR.BRAKECONTROL 0
-->AXIS1.EN
-->BRAKE1.STATE
1
-->AXIS1.MOTOR.BRAKECONTROL 1
-->BRAKE1.STATE
0
Context
For more information see Brake and Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.MOTOR.BRAKECONTROL | 0x500B | 0xC | USINT | - | - | RW | False |
| AXIS2.MOTOR.BRAKECONTROL | 0x510B | 0xC | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|